2025-01-07 1:08 AM
Hello,
We are looking to use VN9D5D20FN (SPI management and monitoring) as power distribution solution for our product. There are 4 channels which are fed from common output of a buck converter. The buck has 5V 3.2A max output and that goes into VN9D5D20FN, to be shared across 4 channels.
VN9D5D20FN datasheet specify minimum operating voltage 4V with a recommended operating voltage of 13V. At 5V we are very close to this min threshold, any considerations?
Thanks.
Cio
Solved! Go to Solution.
2025-01-07 2:55 AM
Hi,
I don't think that 5V is a problem (the undervoltage shutdown limit is 2.7V max.).
You only have to deal with a sightly higher Rds ON (CH 0,1: max. 12.3mOhm, CH2,3: max. 37mOhm @ 4V, 25°C)
Martin
2025-01-07 2:55 AM
Hi,
I don't think that 5V is a problem (the undervoltage shutdown limit is 2.7V max.).
You only have to deal with a sightly higher Rds ON (CH 0,1: max. 12.3mOhm, CH2,3: max. 37mOhm @ 4V, 25°C)
Martin
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.