2019-08-22 10:03 AM
We are using L7805CV ,
Input voltage = 30V
output expected = 5V with 100mA of current requirement
But we are getting 7.5V, the L7805
may know the reason?
according to datasheet input voltage is 35V
Current supplied to the micro controller board and output driver IC,
Still 7805CV not able to deliver the 5V
Please find the attached circuit for the refernce and let us know
please let me know why this circuit is not working or let us know the input voltage limitation of the 7805CV,
Power_supply_30Vin_5Vout_100mA output
2019-08-22 10:20 AM
In the future, post ONCE, don't put the entire question in the TITLE/SUMMARY
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.