2011-11-08 2:01 AM
In my design iam using Viper25DTH.
My o/p power is upto 6W i.e. 4.1V@1.5A. But whenevr i am ging 1W load, the voltage on VDD pin starts to oscillate between 4.5V to 15V and feedback voltage is upto 3.4v, it seems that OLP protection is on at this stage. I have selected Rlimt=18K Rovp=100K Rff=1000K I have done many iterations to achieve o/p but invain. Please suggest #urgent2011-11-14 5:28 AM
2012-01-03 2:34 AM
Sorry for the very late reply.
I have solved the problem. I have coming up with a new problem. 1. Earlier my design was for isolated smps, but i need to make it to non-isolated smps. For this i replaced the opto from circuit and directly connected the output of TL431 to FB pin of viper 25. With doing this my line regulation becomes very poor. I am not able to trouble shoot the problem. Primary inductance :1mH E20 core Switching frequency at no load under above mentioned condition is 28Khz. Please helpWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.