2011-12-26 4:35 AM
Hello.
When activating the
brake
option
I get the following
error.
''
ID211
brake
resistor
switch
off
threshold
voltage
Higher Than
over-
threshold''Dissipative
brake
checked
and
active high
.Min
rated
voltage
18V
Max
rated
voltage
32V
Nominal
voltage
22V
at
sensing
Enabling and
firmware
protection.
enable
overvoltage
threshold
voltage
over
32V
on
over
voltage
switch
on
brake
resistor.
I think that
limit
is in
this parameter.
There is a
parameter
in the file
''drive
parameterers.h
''# define
R_BRAKE_SWITCH_OFF_THRES_V
250
and the
template
''# define
R_BRAKE_SWITCH_OFF_THRES_V
//@@##
TEIDE
%03067
''But
I can not find
how to change
from the program.
?????
Best regards
2011-12-27 1:05 AM
Hello jkin,
that's a known bug of the ST MC Workbench, thanks for your feedback. If you need to use the resistive brake functionality, I think the best you can do is to generate files without enabling the brake and than modify Drive_parameters.h manually. It will be fixed in next release. Happy Holidays, BillinoWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.