Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

L6470 - Vdd Vreg Vs caps, SW input pin voltage

Posted on March 20, 2012 at 18:09Hi! I have some questions about L6470 decoupling and voltage tolerance.1. If I use an external 3.3v to drive both Vreg and Vdd (internal reg disabled), do I still need a 40uf Vreg cap or I can use just one 10uf?2. Ca...

Ats by Associate II
  • 1641 Views
  • 3 replies
  • 0 kudos

HVLED805

Posted on January 06, 2012 at 10:09Hello,I want to execute my project with HVLED805 where input voltage is 176…264 V.Output voltage for LED equal 18 V, output current 0.45 A.Edesign proposed the transformer with widings: Primary – 145 turns, Aux...

ramator by Associate III
  • 1335 Views
  • 1 replies
  • 0 kudos

STM3210E Eval Board Problem

Posted on March 05, 2012 at 16:38STM3210E eval board has a stm32103ZG MCU  on it and this MCU resides in  XL-density group. The problem is related with ST motor control workbench. It has no option to generate header files for XL density devices unde...

ahmetnas by Associate
  • 884 Views
  • 1 replies
  • 0 kudos

STM3210E-EVAL dual motor drive

Posted on February 08, 2012 at 15:30Hallo, is it possible to drive two motors with this eval board? I don't want to drive them simultaneously and independently but ''mutual exclusive'', i.e. I have one enable signal for every motor, while only one ...

STM32 FOC PMSM SDKv3.0 Timer initialisation

Posted on February 15, 2012 at 01:24Hi, I'm working with the PMSM firmware library V3.0 to make a motor control using the STM32F103C8T6 processor operating on my own board. I am working with the provided non-RTOS project which was originally configu...

L6470: Overclocking?

Posted on January 24, 2012 at 08:01Hi We want to overclock the L6470 (10MHz instead of 8MHz at OSCIN) to increase maximum RPM. The resolution will be reduced, this is clear, but is there any other risk to do so? Regards Michael

viper25

Posted on November 08, 2011 at 11:01In my design iam using Viper25DTH. My o/p power is upto 6W i.e. 4.1V@1.5A. But whenevr i am ging 1W load, the voltage on VDD pin starts to oscillate between 4.5V to 15V and feedback voltage is upto 3.4v, it seems ...

sam_niraj by Associate II
  • 1129 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.