2012-05-15 9:08 PM
I have an application where i need to use Viper25H in non-isolated mode.
For reference generation I am using TL431. But the problem is that when TL431 is used for non-isolated configuration , power supply is getting into burst mode operation.
Can you please suggest a reference circuit for using TL431 in non-isolated configuration specifically for Viper25H. The same configuration if used using Opto-coupler its working fine
As Viper25 does not have in it a error amplifier so i cannot used a simple resistor divider.
Using a zener based solution will have more impact on its temperature based tolerances.
So i have to use TL431 in feedback loop but using it for non isolated configuration is a bit of trick. Please suggest its urgent
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.