2017-07-19 2:39 AM
I noticed there are two lib files in Cortex-M4 core MCU:
MC_Library_ProtectedSources_SD_CM4_CCM_MKD.lib and MC_Library_ProtectedSources_single_drive_CM4_MKD.lib
I can't find any description for the diffrence between them, so I should choice which one in my application?
thank you.
2017-07-30 11:43 PM
anyone can help me
2017-11-25 10:03 AM
The CCM Lib makes use of the Core Coupled Memory, functions are executed from RAM (=significantly decreased critical task execution time). See also AN4296 and UM1080
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.