cancel
Showing results for 
Search instead for 
Did you mean: 

Stepper motor moves when touched

allen22
Associate

I'm currently controlling a closed loop stepper motor with an Arduino Uno R3 via the CL86 stepper motor driver. I also connected 2 buttons with pull-down resistors with which I can, for example, rotate the stepper motor by 90 degrees in one direction.

The control works so far, but the buttons also trigger when I touch their cables (e.g. the pull-down resistor) and also the stepper motor (metallic surface).

Why is that the case? Anyone have a tip?

Don`t listen to what other say about you, lead you own life. https://www.oyostepper.de/
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
AScha.3
Super User

Missing ground /earth . So you should care for some ESD/antistatic area, but at least connect circuit ground to mains ground /earth .

And check your supply for correct insulation or let it check by someone, how knows about safety regulations and has the equipment to do a check.

Show a pic, what you have there, including supply.

If you feel a post has answered your question, please click "Accept as Solution".
Techn
Senior III

Make sure that you have connected uno gnd to the drive logical gnd . Try to reduce the button pull down resistor values. 

If you feel a post has answered your question, please click "Accept as Solution".