Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

EVAL-L9963E-MCU firmware & drivers

I am a master's student and working on BMS and I want to use EVAL-L9963E-MCU evaluation board for my research work. But I am not sure whether the firmware or driver for this evaluation board is available in the ST website. Please help me with this in...

L9960 pcb design

 Hey,I'm planning on building an ETC to control a throttle valve using the L9960 H-bridge. I'm currently in the process of designing a PCB for it. The driver is supposed to have 12V as VsV_sVs​ and handle up to 10A max as output load. The PCB I'm des...

DiogoPedrosa_0-1719339031559.png

Resolved! Is the PD85004 part discontinued?

Is the PD85004 part discontinued? We wonder if you have any remaining stock to make the power module with that part.And I was wondering if there are any parts or subsequent parts that are an alternative to that.

jun-min by Associate
  • 1874 Views
  • 3 replies
  • 4 kudos

Schottky Diode for GHz range

Hi, I am working on a project involving input signal in the 3-5 GHz range. For the rectifier circuit, I wanted to use the BAS70-04FILM diode by ST. Is that suitable for the given frequency range though? Else is there any alternative for the same?  Th...

RitooV by Associate
  • 1907 Views
  • 1 replies
  • 0 kudos

STEVAL-L99615C: Why I can not discharge my battery?

Dear ST:Why I can not discharge my battery? Only Charge into it?my setting are below:1、Hardware:CN2 connector:I connect a load(small DC fan,or a resistor)to CH+ CH-;2、Software:In GUI, I run file ( Current Acquistion Init - CC+CSA.csv),      Activate ...

jingbos by Associate II
  • 1888 Views
  • 2 replies
  • 0 kudos

Resolved! Spice model for STB60NF06 mosfet

Hi, I am looking for a spice model for this mosfet (preferably one that runs stable in LTSpice). Purpose is to do some simulations for a SMPS (detailed calculation during transients should be supported by the model). I did not find in STB60NF06 - N-C...

Herwig by Associate
  • 2762 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.