2024-01-09 12:14 PM
I'm designing a automatic fan switch using a BTA26-800CWRG triac. I'm planning on a RCD snubber. All I've seen so far show a single diode across the resistor of the snubber. But it seems if the snubber is snubbing an AC source there should be two parallel back to back diodes to handle both the positive and negative sources. Can anyone confirm or shed some light on the subject? Thanks.
Solved! Go to Solution.
2024-01-10 1:05 AM
Welcome @Rod, to the community!
Unfortunately, you have not given any sources where you have found such a structure with a diode. If a snubber is required (the BTA26-800CWRG is a so-called snubberless TRIAC), then it is normally inserted as an RC element (see e.g. AN437).
Regards
/Peter
2024-01-10 1:05 AM
Welcome @Rod, to the community!
Unfortunately, you have not given any sources where you have found such a structure with a diode. If a snubber is required (the BTA26-800CWRG is a so-called snubberless TRIAC), then it is normally inserted as an RC element (see e.g. AN437).
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.