Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Cannot connect STWBC86 to WPSTUDIO V1.8.4

Hi there, we are trying to operate a STWBC86 on a rebuild of STDES-WBC86WTX.Eval boards are not yet available so we needed to build them with the given data on our own. when powering it up nothing happens so i assumed i need to program the supplied F...

S3rr4_1-1700116881021.png S3rr4_2-1700117000992.png
S3rr4 by Associate II
  • 2768 Views
  • 3 replies
  • 1 kudos

Resolved! Wireless Power Solution Needed

Wireless Power Requirements:-Require 5W on Receive side-Active Part Number and industrial temp rated-Air Gap: 20 to 30mm but ideally up to 40mm-Coil Size: 50mm or smaller is ideal, room to adjust size as needed-Don’t need to be compliant with any oth...

PNada.3 by Associate II
  • 1488 Views
  • 1 replies
  • 0 kudos

Resolved! Questions on wireless charger receiver STWLC38

Hello!I would like to get information on the wireless charger receiver Part no: STWLC38.I am looking for a wireless power receiver that supports:10.5V-11V voltage output0.65A current outputSTWLC38 - per the datasheet it appears to support the above r...

MK.12 by Associate II
  • 1958 Views
  • 1 replies
  • 1 kudos

Resolved! DTS on the STWLC38

What is DTS used for?And can I configure the following set of registers on through I2C to send and receive data in-between 2 STWLC38s through the main coil ? Does this Qi IC have a detailed user maual? 

baymax_0-1699517265439.png
baymax by Associate
  • 1274 Views
  • 1 replies
  • 1 kudos

Spice/ibis models for power ICs

Hello,I'm looking to incorporate component models for L6924D and SPV1040T into Altium Designer for PDN analysis and simulation. Are there any available model files for this purpose?

Levan by Associate III
  • 787 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.