2025-12-02 2:13 AM
Hello,
are there any example parameters available to drive a stepper motor fast in current mode? I am using the EVLPOWERSTEP01 evaluation board with different stepper motors, e.g. Oriental PK267JDA (3.4V, 2.8A, 1.2Ohm) and Nanotec ST6018K2008 (4.8V, 2.0A, 2.4Ohm). Every motor stalls at 9 rev/sec. I used the settings related to UM1829 and played with all parameter values. Without any progress. How to speed up to e.g. 60 rev/sec?
I attached my default parameters from the SPINFamily tool.
Thanks in advance,
Stephan
Solved! Go to Solution.
2025-12-04 12:42 AM
2025-12-04 12:42 AM
Solved
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.