Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! powerSTEP01 advanced current control parameters

Hello,are there any example parameters available to drive a stepper motor fast in current mode? I am using the EVLPOWERSTEP01 evaluation board with different stepper motors, e.g. Oriental PK267JDA (3.4V, 2.8A, 1.2Ohm) and Nanotec ST6018K2008 (4.8V, 2...

LD1117 Input & Output Capacitor requirements

I am currently designing a circuit using the LD1117S50CTR.In the recommended circuit in the datasheet, Cin = 100 nF and Cout = 10 µF are specified.For an LDO, I believe Cout is critical, while Cin is not as important.Therefore, I am considering using...

Matsuura by Associate II
  • 1253 Views
  • 8 replies
  • 1 kudos

Example Code for VNF1048F

Hello ST Community, i have problems to get the VNF1048F chip to run. It goes every time to the fault state and can not find out, why this problem occurs.The documentation for this chip is not really good and there is not sample application (Source Co...

Markus_W by Associate
  • 1411 Views
  • 4 replies
  • 1 kudos

VNF1048F & VNF1248F SPI Communication without VS

Hello, We are developing a design around VNF1048F & VNF1248F products.  We are considering a multichannel design with different output settings. In a multichannel design, naturally we are expecting to have control and monitoring capability of individ...

zekasi by Associate
  • 216 Views
  • 0 replies
  • 0 kudos

VNF1248F & VNF1048F Functional Safety

Hello,We are developing a design around VNF1048F & VNF1248F products. From the other community posts, we learned that VNF1048F has ASIL - B for functional safety rating.We would like to confirm this information, and we also would like to know if VNF1...

zekasi by Associate
  • 231 Views
  • 0 replies
  • 0 kudos

L6494LDTR

Hello I am using the L6494(14PIN) as a driver for a high and low side FET in a half bridge arrangement. My DC volts can be anything from 120Vdc to 220Vdc. and current up to 17AIs there anyway to determine the breakdown mechanism if I do not momentari...

camabe by Associate
  • 2158 Views
  • 1 replies
  • 0 kudos

EVLVIPGAN65DF radiated EMI

EVLVIPGAN65DF application note states that the provided reference design is compliant with IEC55022 Class B conducted EMI. How about radiated EMI? Is there any measurement in this regard? 

Gaston by Senior
  • 663 Views
  • 4 replies
  • 0 kudos

Resolved! L6982CDR application problem.

Hi,We're encountering an issue with the L6982CDR buck converter in our application. Here's the detailed scenario: Configuation: We're using it to convert a 24V input to a 5V output to power the board. Load: The 5V output supplies a load current of ap...

PL3_1-1760668895581.png PL3_0-1760668869816.png
PL3 by Associate II
  • 1747 Views
  • 12 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.