2025-09-21 2:47 AM
I was design 19 volt regulated power supply, but I don't know the exact value for the transistors, and I noticed at the voltsim output didn't reach the maximum 19 volt output, can anyone help me for the solution for my design, regards.
Solved! Go to Solution.
2025-09-21 7:11 AM
The schematic shows a current regulator that uses the potentiometer as a shunt. However, if your output parameters are actually 19V, 20A (even though you have drawn 1.9V), there would have to be 20,000V at the 1k potentiometer (20A * 1k = 20kV).
Please explain what your schematic is supposed to do or what you are connecting there, because (at least) something about it is not right.
Regards
/Peter
2025-09-21 6:17 AM
Why using a fixed 8V reg for a 19V supply ?
+
You have planned the cooling ? (need a big heatsink, + fan probably )
2025-09-21 6:45 AM
Actually what you've designed is a big heater with an annoyingly bright lamp.
2025-09-21 6:53 AM
2025-09-21 7:11 AM
The schematic shows a current regulator that uses the potentiometer as a shunt. However, if your output parameters are actually 19V, 20A (even though you have drawn 1.9V), there would have to be 20,000V at the 1k potentiometer (20A * 1k = 20kV).
Please explain what your schematic is supposed to do or what you are connecting there, because (at least) something about it is not right.
Regards
/Peter
2025-09-21 7:32 AM
@Peter BENSCH thank you so much for your help, well I see my pot act as a shunt instead as voltage divider. and I guess my 1k pot will give me 13.8 volt at half turn for my Dakai transformer and also can be used to turn my Laptop on at max. turn.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.