2016-06-01 12:04 AM
Hello guys,
I have been working on stepper controller board using L6482 chip, but with no luck making it to work..Problem: I'm getting over-current fault when I try to drive the motor (motor doesn't make any movement).Controller settings:TON_MIN = 4us,TOFF_MIN = 21us,TOFF_FAST = 10us,FAST_STEP = 16us,TSW = 48us,Predictive current control is ON,Gate current = 16mA,VCC value = 15V,UVLO tresholds = 7V,Turn OFF boost time = Disabled,Controlled current time = 1500ns,Blanking time = 500 ns,Dead time = 250 ns,All currents set to 195.31mV,Over-current treshold = 750mV.Power supply = 36V, 11A (SMPS)Mosfets I'm using: IPP180N10N3G, Qg= 19nC (25nC max)Stepper: Nema 23, 0.9 Ohms, 3.8 mH.I need to deliver max 4.5 Amp to the motors. Speed should be around 400steps/s at 1/16 microstepping. I have tried to set very low current setings for the motor but stil nothing is happening.. PCB is made with using EVAL 6482 as a reference, only MOSFETs are different. Looking forward for your answer!Thank you!Julius K.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.