Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

L6482H settings.. What I'm doing wrong?

Posted on June 01, 2016 at 09:04Hello guys,I have been working on stepper controller board using L6482 chip, but with no luck making it to work..Problem: I'm getting over-current fault when I try to drive the motor (motor doesn't make any movement)....

Startup issue with HVLED001 demo board (STEVAL-ILL069V1)

Posted on May 25, 2016 at 10:08I am evaluating HVLED001 IC’s demo board (STEVAL-ILL069V1) which I found that such demo board have difficulty to power up if the output is loaded (even as low as 50mA). To operate the board I have to power up the unit ...

cheehhow by Associate
  • 758 Views
  • 0 replies
  • 0 kudos

L6470 Cannot change Step Register

Posted on May 23, 2016 at 03:43i have eval6470PD R1.1 connected to STeval-PCC000V2 running spin software.each time i try to change default register of 7 ( 1/128sep ) to full value of 0,it does not work either with reg write button or explicit WR but...

STEVAL - IHM034V2 how to start a three phase motor

Posted on May 11, 2016 at 13:01Hy,I took a this board and delete firmware from the microcontroller, and I try to develop a my firmware for motor control, but I have a problems, the motor won't to start. Now, what signals I need to send on full bridg...

emir by Associate
  • 618 Views
  • 0 replies
  • 0 kudos

Question about L6480 BUSY/SYNC pin SYNC output

Posted on May 03, 2016 at 15:27Hi all,Regarding to L6480 datasheet, STEP_MODE register has SYNC_EN bit and SYNC_SEL. if SYNC_EN bit is set high, then SYNC output provides a clock signal according to the SYNC_SEL parameter. the sync signal is obtaine...

cliang by Associate II
  • 1079 Views
  • 1 replies
  • 0 kudos

SLLIMM SDIP-25L package drawing

Posted on May 04, 2016 at 03:35Is there a more detailed drawing of the SLLIMM SDIP-25L package than what is on the corresponding power module's datasheet?  Or is there a suggested footprint for the SDIP-25L?

Project Example

Posted on January 27, 2015 at 16:55Hi, would be possible to share some ready made simulation configuration to get used to this new tool? Thanks #twistersim #examples #examples

marte by Associate
  • 1375 Views
  • 2 replies
  • 0 kudos

STWBC - SWIM interface

Posted on May 03, 2016 at 01:34Is the SWIM interface available for Flash and EEPROM programming? It seems this device contains a STM8 controller. I am wondering if the std SWIM interface is fully available for memory access. Thx #stwbc-stm8-swim

musche by Associate
  • 756 Views
  • 0 replies
  • 0 kudos

EVAL6474PD does not transmit any voltage impulses

Posted on April 22, 2016 at 13:23Hello, I am using EVAL6474PD demonstration board with PCC009V2 controller for stepper motor. Also I have spinfamily evaluation tool 3.0 . The problem is that stepper motor does not recieve any impulses. I cheched it ...

simas by Associate
  • 701 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.