Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

EVAL6470H Application

Posted on June 06, 2012 at 22:38Hi,I'm currently evaluating the L6470 for a mobile robot application using the EVAL6470H demo boards. I've been able to get my differential drive motors running and now I want to perform 2 tests to mimic real world sc...

dttworld by Associate II
  • 1295 Views
  • 4 replies
  • 0 kudos

Setting up FOC for a small BLDC-motor with hall sensors

Posted on June 18, 2012 at 13:30Hi I am trying to setup the ST FOC library with a small BLDC-motor with hall sensors. I am using the evaluation board STEVAL-IFN003V1. I have configured all parameters of the system with the ST Motor Control Workbenc...

fortunat by Associate II
  • 3649 Views
  • 6 replies
  • 0 kudos

12V / 6A Power supply. Help with Buck and Boost converters

Posted on June 07, 2012 at 15:05Hello all.I would like to receive some suggestions of ICs / considerations about this design.The picture below states how this power supply should work.http://e2e.ti.com/cfs-file.ashx/__key/communityserver-discussions...

STM32 FOC PMSM SDKv3.0 : Driving different motors

Posted on March 22, 2012 at 02:32Hi I have several different motors that I would like to drive (one at a time) using the same hardware and firmware based on the STM32 FOC PMSM libraries. The motor selection is indicated to the processor with a DIP s...

Non-isolated configuration in Viper 25

Posted on May 16, 2012 at 06:08I have an application where i need to use Viper25H in non-isolated mode.For reference generation I am using TL431. But the problem is that when TL431 is used for non-isolated configuration , power supply is getting int...

Simulation for L6599 in eDesignSuite

Posted on April 28, 2012 at 08:56Hi all, I got a 200 Watt Resonant SMPS board based on L6599 (STEVAL-ISA018V1) and wanted to  simulate it with the eDesignSuite but I couldn't find a L6599 design. It seems that there are no eDesigns for the L6599 ava...

HALL Timer on STM3210B-EVAL

Posted on April 11, 2012 at 16:34Hello, I'm a bit confused about the timer usage for the Hall sensors on the STM3210B-EVAL board. The encoder signals (which are used for the hall signals too) are placed on the GPIOs PA0, PA1 and PA2 and timer TIM2 i...

VIPER53E design software

Posted on April 10, 2012 at 02:44The new eDesignstudio does not support the VIPER53E. Original design was done by software supported by ST, but can not find it on the web. Can you send me or point me to where I can get a copy?

Speed adjust for L6207

Posted on March 19, 2012 at 10:50Hi everybody On my simple Cw, Ccw control, for low power brushed d.c. motors, realized around L6207, i need to adjust the motor's speed. Is it a good idea to Pulse Width  modulate the enable input (EA) instead using ...

apoggiali by Associate II
  • 2443 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.