2012-02-14 4:24 PM
Hi,
I'm working with the PMSM firmware library V3.0 to make a motor control using the STM32F103C8T6 processor operating on my own board. I am working with the provided non-RTOS project which was originally configured for the STM3210B-EVAL board. I have the problem that timer 1 apears to be remapped (AFIOMAPR:TIM1_REMAP = 0x3) regardless of definition: #define PWM_TIMER_REMAPPING PWM_NO_REMAP in the Control stage parameters.h file. Edit: Problem solved by using the Batch build option to re-compile the motor control code instead of just Download and Debug which only recompiles the user project. Thank you Nick2012-02-15 7:24 AM
Hello Nick,
r you using the PC Tool STMCWB (ST MC Workbench) for the generation of Control stage parameters.h file? Can you share the ST MC Workbench configuration file? Regards, Billino2012-02-15 12:09 PM
Hi Billino,
Thank you for your prompt reply. I originally generated the Control stage parameters.h file with ST MC Workbench for the STM3210B-EVAL board and then modified them by hand for my hardware. Actually I have already solved the problem: I had not used the Batch Build function in IAR Workbench after modifying the .h files. Once the software was re-built with the Batch Build function it began to work correctly. Thank you, NickWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.