Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

L7805 regulator decoupling capacitro faulier

Hi Sir/Madam, My application is photoelectric sensor object detection or object sensing. I am using the L7805 ST make. Positive voltage regulators output voltage is 5V, and I am giving the input voltage as 24V, and the maximum DC voltage is up to 30V...

Resolved! l6566bh based flyback converter ground short together

hi all,     i am designing flyback converter based on the l6566bh. i have 2 outputs on the secondary side, both are separate windings (different ground potential) in transformer. can i short together for shared ground reference if isolation is not ne...

Need model simulation for IGBT

Hello ST team,I would like to have SPICE model for STGHU30M65DF2AG and for STGSH80HB65DAG. I've advised to try with eDSim, however I did not find the model in that. BR,Siva

s_sk by Associate
  • 726 Views
  • 1 replies
  • 0 kudos

PWM current LED PCB with STCS2A

Dear all, I received a LED PCB with 16 STCS2A constant current LED drivers in parallel, each powering 4 LEDs. Vcc=12V, for the PWM signal a 5V signal is used, which is supplied as follows: 24V PWM output of PLC is coupled to an optocoupler which is c...

wdh by Associate II
  • 1796 Views
  • 4 replies
  • 0 kudos

Resolved! Transformer Design in AN2794 for Push-Pull Converter

Hello,I’m designing a 1 kW converter using a push-pull topology with 24 V input and 400 V output. While doing so, I referred to the transformer design guidelines in your document AN2794. Unfortunately, I believe there are some inconsistencies or erro...

Nafi-Can by Associate II
  • 4823 Views
  • 9 replies
  • 0 kudos

Resolved! PLECS Model of stgwa50ih65

Hello- I am working on simulating a resonant converter based on stgwa50ih65. Can you please share its PLECS model? I am unable to find it on its website. Thanks!

Sid_RWTH by Associate
  • 1016 Views
  • 1 replies
  • 0 kudos

Resolved! STUSB4500 Debug Accessory Mode

 Hello,We are currently developing a couple of devices with USB-C DAM support and have chosen to use the STUSB4500 as the power sink on the device side.We would like to understand whether the following behavior is expected, and if there are any optio...

Screenshot 2025-05-21 115521.png
Andrius1 by Associate
  • 1127 Views
  • 1 replies
  • 1 kudos

About STUSB1602 SPI and I2C register description

I am planning to use the STM32WBA62 to interface with the STUSB1602 USB PD controller to implement both dual power role and dual data role functionality. However, I do not have the I²C or SPI register documentation required for development. Could you...

CY_Tsai by Associate III
  • 672 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.