2025-05-23 3:21 AM - last edited on 2025-05-23 4:36 AM by Andrew Neil
We are currently evaluating two ST IPM modules for our motor drive applications — STGIB8CH60TS-E and STGIB15CH60TS-L. Upon reviewing both datasheets, we noticed that although the two devices share the same functional pin descriptions where (STGIB8CH60TS-E have max current of 12A @ 25°C) and (STGIB15CH60TS-L have a max current of 20A @ 25°C) but package types are different, the physical layout of certain pins, specifically Pin 19 (NV), differs between the two modules.
We would appreciate your clarification on the following points:
What is the technical reason for the difference in Pin 19 layout between the STGIB8CH60TS-E (Type E package) and STGIB15CH60TS-L (Type L package)?
Are there layout-compatible alternatives to STGIB8CH60TS-E (i.e., IPMs with similar electrical characteristics and identical physical pin positions) that could support higher current or allow for flexible sourcing?
Solved! Go to Solution.
2025-05-23 4:28 AM
Welcome @VishnuNatarajan, to the community!
The extended pin 19 was probably introduced at the time at customer's request.
The STGIB8CH60TS-E is the only remaining variant with this layout in the portfolio of STMicroelectronics.
Does it answer your questions?
Regards
/Peter
2025-05-23 4:28 AM
Welcome @VishnuNatarajan, to the community!
The extended pin 19 was probably introduced at the time at customer's request.
The STGIB8CH60TS-E is the only remaining variant with this layout in the portfolio of STMicroelectronics.
Does it answer your questions?
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.