Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

A7986A DC-DC Design not working

Posted on April 26, 2016 at 13:07Hi to all,please help!!I made a DC-DC converter from 9-30V input and 5V output. You can find in the attachment a pdf print from the eDesign Suite.The Cin that I'm using is: C1210C335K5RACTUThe L is: B82477G4153MThe C...

Minimum working voltage of VIPer12A

Posted on April 25, 2016 at 08:45Hi all, We are using VIPer12A in our Flyback isolated SMPS. The circuit starts at minimum 20Vrms. There is no information about the minimum Vrms value that the IC starts. The datasheet says IC starts working Vddon wh...

mustafa2 by Associate
  • 805 Views
  • 0 replies
  • 0 kudos

L200 Advice Please

Posted on April 24, 2016 at 10:36Hi New to this forum, Sorry if I have posted this in the wrong place. Is it possible to use fold back current limit on a L200 regulator ? Is there an example circuit that I can look at ? Thanks Steve Clarke #l200

L6491 Evaluation Board

Posted on April 21, 2016 at 22:26Hello, I am testing the L5491 Evaluation board and having problems getting the IGBTs to turn on. Currently I am using FGH60N60 IGBTs for controlling a light bulb. I have a microcontroller generating a 1kHz 5Vpp squa...

eprast by Associate
  • 724 Views
  • 0 replies
  • 0 kudos

Run mode power consumption of STM32L053R8 at 16MHZ?

Posted on April 20, 2016 at 14:06Hi,I'm new bee here. My project needs to consume very less power. I see that STM32L053R8 consumes 88µA/MHZ that means it takes 88µA*16 for 16MHZ? or is it different?. I would like to perate my controller at 5MHZ only...

gandhi by Associate II
  • 833 Views
  • 0 replies
  • 0 kudos

EVAL6480H and catch/snubber diode omission

Posted on April 18, 2016 at 21:49Hello, EVAL6480H uses very robust MOSFETs with hefty intrinsic diodes (25A pulsed current). Does this suggest that it would be ok in practice to exclude catch/snubber diodes from H-bridge design when employing the L6...

SPV1040 Breakdown

Posted on March 17, 2016 at 11:26Dear all,we are noticing breakdown of SPV1040 in our implementation on a board for energy harvesting from solar panel. The breakdown is only for some board. Here you can see the configuration.The solar panel is a cou...

0690X00000602gSQAQ.jpg
perla by Associate
  • 1004 Views
  • 1 replies
  • 0 kudos

L6598D spice model

Posted on April 14, 2016 at 08:29Hello, where can I find the spice model of L6598D? I really appreciate it and thanks in advance! Regards Ras #l6598d-spice-model-.subckt-.mod

STEVAL-ISV020V1 / AN4397: SPV1050 MPPT description error?

Posted on April 14, 2016 at 08:08In the http://www.st.com/st-web-ui/static/active/en/resource/technical/document/application_note/DM00100185.pdf?sc=an4397 of SPV1050 evaluation board ISV020V1 the equation of MPPT ratio is given as MPPratio * Voc= (V...

otso by Associate
  • 688 Views
  • 0 replies
  • 0 kudos

PM8800A power Mosfet

Posted on April 13, 2016 at 16:52Hi, I'm using PM8800A in isolated topologies, 5 Vout with synchronous rectification. I followed the directions of Application notes AN_2783 and used the STS26N33LLH6 transistor output from the transformer. The proble...

afucini9 by Associate
  • 760 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.