Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Nucleo ihm001

Posted on March 30, 2016 at 20:21 Anyone had any luck getting the example project compiled and running for the Nucleo-IHM001? The binaries work fine respectively in both 6step and FOC modes. However when the example provided with SPN7V1.0.0 is c...

SPI Comm between STM32F103 micro and EVAL6470H board

Posted on November 12, 2015 at 21:17When I send any get or set command from micro to L6470 via SPI, the L6470 always responds with the command byte sent by the micro. It should be either sending the MSB of the get data or a 0 byte for a set command ...

L6226Q broken when Vs pin is rapidly switched on and off ?

Posted on April 13, 2016 at 11:48Hello, I am using the eval board EVAL6226QR that has the dual full bridge driver L6226Q on it. I am using it to drive a 40kHz train of pulses from IN1A to OUT1A (and IN2A to OUT2A). To minimize current consumption, I...

mahmoud2 by Associate
  • 854 Views
  • 0 replies
  • 0 kudos

Voltage drop in L6205

Posted on April 13, 2016 at 11:27Hallo..I am using L6205 in parallel connection mode for high current. I have attached a load resistance of 10ohm at output and the Supply voltage is 12 volt. The load resistance was drawing about 1.2Amp current and I...

L6208 PWM Current Control

Posted on April 13, 2016 at 10:22Need help with calculation parametrs for current regulator.Try to use AN1451. And can`t calculate Switching Frequency.How to know Toff parametr ?

timohin by Associate
  • 671 Views
  • 0 replies
  • 0 kudos

230VAC 50HZ to 12VDC 200mA PSU

Posted on April 01, 2016 at 18:07Hello Members,I have recently started looking into designing an AC/DC converter with the rating as mentioned in the subject. I am looking into possible solutions or reference designs provided by ST for this purpose. ...

230VAC 50HZ to 12VDC 200mA PSU

Posted on April 01, 2016 at 18:06Hello Members,I have recently started looking into designing an AC/DC converter with the rating as mentioned in the subject. I am looking into possible solutions or reference designs provided by ST for this purpose. ...

Motor voltage feedback.

Posted on January 10, 2016 at 17:24Now that I have FOC working on the STM board and the STM ''power stage'' the next step is to move all this over to my own power stage and logic board. The CPU part can wait, so now I'm working on getting the nucleo...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.