Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

What kind of impact can demage the L6470pd in that way?

Posted on June 27, 2016 at 13:35Hi at all, is there someone with an idea what has happened there with the L6470. I´ve attached 2 photos of the demaged device and on picture of the scematic sheet. It looks like the motor bridges are directly shorted ...

dbecher by Associate
  • 1028 Views
  • 0 replies
  • 0 kudos

[STM32F10x] Timer 1 overflow/underflow not correctly

Posted on June 26, 2016 at 07:06Hi everyone,I'm building a BLDC motor control project which use 6 steps for control. And now, i wanna sample ADC on timer1 overflow when PWM-ON (PWM run in PWM mode 1 and Center-Aligned3). I get an issue: Timer 1 over...

L6480 SPI errors versus gate drive configuration

Posted on June 20, 2016 at 08:23Hi, I designed a board equipped with two L6480 motor drivers; the drivers are connected in daisy chain mode. To keep the two motor synchronised, the OSCout of the first driver of the chain feeds the OSCin of the secon...

evalL6474PD not working

Posted on June 17, 2016 at 22:37 i bought two different ST motor eval boards connected to the STEVAL-PCC009V2; eval6470PD and eval6474PD. the eval6470PD works fine but i want to use the eval6474PD for technical reasons ( current vs volt control). th...

L6491 Dev Board Control

Posted on June 15, 2016 at 17:24Hello again,As an update I got my Development Board working blinking a light. I noticed that increasing the pulse frequency in HIN/LIN causes the Gate pulse width to change. The input is symmetrical to the output unti...

eprast by Associate
  • 667 Views
  • 0 replies
  • 0 kudos

STBCFG01 and the eval board software

Posted on June 14, 2016 at 22:06Where can I download the eval software for the STBCFG01 eval board? It seams to be hidden very very well. It's why I bought this board... Thanks, Kevin

kbkibbe by Associate II
  • 512 Views
  • 0 replies
  • 0 kudos

L6474: Can only see pulses on one of the phases?

Posted on July 15, 2015 at 22:01A colleague and I noticed something unusual when we were using an L6474 to drive a stepper motor.When the motor was stationary, we observed pulses on both of the motor phases.  This presumably corresponds to the PWM p...

dvelasco by Associate II
  • 875 Views
  • 2 replies
  • 0 kudos

Output current SPV1050

Posted on June 09, 2016 at 21:19Hi everyone.Here there is my easy question.How is it possible to charge the battery at the maximum current (70mA)?Actually my solar panel can provide more power than the SPV1050 can use, however the  charging current ...

LED7708 4-wire protocol

Posted on June 02, 2016 at 09:30Hello, The 4-wire protocol of the LED7708 chip is not clearely explained in the doc. I cannot get it to work. The STEVAL-ILL035V1 board describes all the electrical parts, schematics, but nothing about protocol and pr...

yvan2 by Associate
  • 655 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.