2016-05-30 6:18 PM
From the literature, the abs_pos value is a 22 bit 2's complement integer. but when i move the position above 32768 (16 bit 2s complement maximum), the value resets to negative. I.e. the abs_pos value acts as a 16 bit 2s complement value.
Additionally, using the dSPIN_Move command and using the dSPIN_BUSY to check to make sure it's finished with the move, the busy pin will go high early and the move will not finish. I.e. i will send a dSPIN_Move(''FWD'',4000) and it will only move so far, then stop without completing the commanded move from the abs_pos before the dSPIN_BUSY goes high. Has anyone else has these issues? Some guidance would help, besides these issues, the product works great.attached is data output from the abs_pos (see line 28774 for example of it ending early) and sample code of how i'm commanding it. #l64702016-12-19 6:29 PM
I had the same problem. In my case, I used the ATmega324 as the master device. CPOL and CPHA of SPI were wrong. After CPOL and CPHA were set 1, the abs_pos has been read properly.
2017-01-20 1:40 AM
Hi,
I'm not able to download the attached file, so I cannot check it, but the behavior seems in some way related to how the micro is interpreting the ABS_POS register value.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.