Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STP16CPC26 SDO output stuck low

This is our first board design that uses the STP16CPC26. We have two chips daisy-chained together. The SDO output from the first chip never goes high. The SDO pin is definitely not shorted to ground or any other net, and is definitely connected to th...

DSudo.2 by Associate III
  • 783 Views
  • 1 replies
  • 0 kudos

Resolved! STP16CPC26 won't do anything

My apologies if this is the wrong ST forum... it seemed like the closest one to the part I'm using.I have a new STM32F072 board design that has a STP16CPC26 LED driver connected to one of SPI busses. I just could not get the chip to do anything using...

DSudo.2 by Associate III
  • 1454 Views
  • 9 replies
  • 1 kudos

Resolved! MOS FET with built-in TVS diode.

I want help to understand this. The STM MOS FET STP6NK60ZFP has a MAX gate-source voltage (Vgs) at 30V. In order to protect it from ESD it has a built-in TVS diode. Over 30V it can fail. But the bulit-in TVS has breakdown voltage (Vbr) set at 30V. It...

ScreenShot_20250620014544.jpeg
Steam by Associate II
  • 1713 Views
  • 6 replies
  • 0 kudos

Resolved! PowerFlat 8x8 HV NC pins

Hi ST Community! I'm working in a HV power design (400VDC) with a STPSC6H065DLF Schottky diode. I can see from its datasheet that pins 1 and 2 are not connected internally, but I can't find any recommendation about what to do with those pins. Would i...

jcarrizo_0-1750361952776.png
jcarrizo by Associate
  • 1347 Views
  • 4 replies
  • 1 kudos

Resolved! VN920SP-E replacement

Hi all,I was wondering if there is any pin to pin replacement for VN920SP-E?VN920SP-E is obsolete now, and one of our main products needs this to function.Any help would be appreciated. 

IWG by Associate
  • 3764 Views
  • 9 replies
  • 3 kudos

LED Drivers - audio product - no noise (no PWM)

Dears, I'm working on an audio project, and I'm searching for LED drivers with no PWM, to avoid noise. I need one sink (common anode LEDs) and one 'voltage' (common cathode LEDs) driver.  Could you please suggest two  drivers, which could comply with...

Matbonny by Associate III
  • 2042 Views
  • 8 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.