2025-06-02 11:57 PM
can PG pin of ST1L08SPU33R be left floating if unused?
Datasheet does not specify it.
Solved! Go to Solution.
2025-06-03 2:24 AM
This is also stated in the data sheet, table 2: VPG = -0.3V ... VBIAS+0.3V. So, pull it to VBIAS.
Good luck!
/Peter
2025-06-03 12:10 AM
Welcome @shubhangi, to the community!
It is indeed mentioned a little hidden. However, the data sheet, table 4, states Isink = 6 mA open drain output for PG. This pin is therefore an open drain output and can therefore remain completely unconnected.
Hope that answers your question?
Regards
/Peter
2025-06-03 1:14 AM
Hi Peter,
Thank you for your response. It indeed is hidden. :)
If I want to use this pin, I assume, I will have to pull-this up. Which voltage rail should it be pulled-up to?
Thanks,
Shubhangi
2025-06-03 2:24 AM
This is also stated in the data sheet, table 2: VPG = -0.3V ... VBIAS+0.3V. So, pull it to VBIAS.
Good luck!
/Peter
2025-06-03 2:28 AM
Thanks Peter.
Regards,
Shubhangi
2025-06-20 12:55 AM
Hello Peter,
Can this IC ST1L08SPU33R handle 3.3V input? i.e. convert 3.3V to 3.3V?
Actually I have a case where input can be either 3.3V or 5V. 5V to 3.3V can work. How about 3.3V to 3.3V?
Thanks,
Shubhangi
2025-06-20 1:14 AM
Well, it is an ultra low drop regulator, but there is still some dropout voltage: the data sheet mentions max 120mV for the whole temperature range, in your case resulting to 3.18V.
2025-06-20 5:23 AM
Hi Peter,
Yes Thats expected. I think 3.18V should work. Thanks.
Thanks,
Shubhangi
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.