Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
HeyWe are using the STBC08 to charger a LiPo battery, the device charges to 4.2v which is the maximum voltage for battery, However I understand that charging to 100% is not optimal in terms of battery lifetime, and most sources recommend not charging...
I am using the STPS5L60U in a low voltage landscape driver design. Input is 9-15Vac. Circuit is a buck-boost. Driver chip is a TI LM3429, driving an external FET. Switching frequency is only 145kHz. COB load is 20V and 750mA. I use 4 of these d...
Hi, i tried LM3424 demoboard and adjust to me purpose. All works perfect, but when i design my PCB and i put all the components, the waveform and the efficiency of the system changes, the waveform of the transistor on the drenator pin is differents b...
as per the figure we provides a dc voltage as a input to the interleaved active clamp flyback converter block, provide a PWM signal to the MOSFET which is in interleaved block for switching purpose. PWM signal is generated by the microcontroller whic...
I tried to download a program for motor control. I think that this is the potential problem because I use wait(1) instead of wait(0.1)
Hi I am having a strange issue with STC3115.My system is designed in such a way that the main MCU and all circuitry is powered using a push button controller. On long press my MCU and all devices will be off but except the fuelgauge which is powered ...
I´m using a PWM signal and the complementary with TIM1(timer1). The Pwm´s complementary singal is going out from pin A7 then I want to turn off the pwm signal from that pin and turn on a HIGH value (one) in the exact same pin (A7). The thing is that ...
@Claire OKU @cedric H @Giuseppe Scuderi_O @brk
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.