2019-11-13 12:06 PM
I´m using a PWM signal and the complementary with TIM1(timer1). The Pwm´s complementary singal is going out from pin A7 then I want to turn off the pwm signal from that pin and turn on a HIGH value (one) in the exact same pin (A7).
The thing is that I can´t do that using HAL_GPIO_WritePin(), I think that is because of the port is not in GPIO mode.
Can somebody help me please?
That would be really helpfull.
I have got a STM32F103C8
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.