2019-11-19 9:02 AM
Hey
We are using the STBC08 to charger a LiPo battery,
the device charges to 4.2v which is the maximum voltage for battery,
However I understand that charging to 100% is not optimal in terms of battery lifetime, and most sources recommend not charging above 90%,
Was that being taken under considerations when designing this product?
I am considering limiting the charging myself but on the other hand don't wish to interfere with the function of an already tested charging device
I would appreciate any insights on this issue.
Thanks!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.