Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Can L9788 be interfaced to a microcontroller via SPI?

Hello all, this post just to know if the L9788 Automotive Engine Management System IC can be interfaced to a microcontroller via SPI instead of MSC bus (single ended interface instead of differential one).Thanks a lot,Regards.AC.

AlxCrt by Associate II
  • 881 Views
  • 9 replies
  • 1 kudos

STPSC10H12G-TR Replacement

Hello,STPSC10H12G-TR is used in our projects, it's NRND and may be going to EOL.Do you have recommended replacement for this part? Thanks!

Cecilia by Associate II
  • 706 Views
  • 5 replies
  • 1 kudos

No LDO output on STEVAL-ISV020V1

Hello,I'm currently evaluating STEVAL-ISV020V1 using AN4397 and I'm not reading any voltages from both LDO outputs.Here's my setup:PV_in: 2.6-2.7 V PVBATT: 5v supercapSW1 and SW2 enabledI can confirm that the supercap is charging as STORE shows ~3.9-...

Resolved! L9963 Voltage measurement problem

I am testing the board with a 14s Li-ion battery, but I am unable to read the cell voltages or configure any register through the GUI. I shorted the X1 and P2 power supply inputs and supplied 12 V to both. This was the only setup in which I could get...

nicim by Associate II
  • 945 Views
  • 1 replies
  • 0 kudos

Need support related to L9305 valve driver bringup

We are currently using the L9305 IC to drive solenoid contactors in our project. The hardware configuration follows the specifications provided in the datasheet.We are able to communicate with the device via SPI and read all registers. However, we ar...

sharanP by Associate
  • 570 Views
  • 1 replies
  • 0 kudos

SPV1040T stays ON and passing voltage from output to input

Hi,Below is the setup I'm using. An SPV1040 connected to a small 2Vmp solar panel charges two 50F supercapacitors connected in series up to Vout = 4.8V. The design is taken from the AN3319 application note of the STEVAL-ISV006V2. Currently, I have ma...

asdafsd.PNG
NEche.1 by Associate II
  • 1431 Views
  • 1 replies
  • 0 kudos

Resolved! ACST series

I would like to use the ACST series as an AC switch for a 90kHz AC capacitive load. Is this possible?

STOMO.11 by Associate
  • 998 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.