2025-08-19 6:36 AM - edited 2025-08-25 3:36 AM
We are currently using the L9305 IC to drive solenoid contactors in our project. The hardware configuration follows the specifications provided in the datasheet.
We are able to communicate with the device via SPI and read all registers. However, we are facing the following issues:
We have reviewed the SPI frame format and CRC, and everything appears correct. Could you please advise on:
Any guidance or recommended steps to resolve this would be greatly appreciated
2025-08-25 1:32 AM - edited 2025-08-25 1:34 AM
Hello,
I have uploaded the SPI data. After initialization, I am pulling the EN_DR and nRES pins from low to high via GPIO, and then starting to read all registers. You can refer to the data in the uploaded Excel file. However, some of the register values are not as expected.
Your prompt response would be helpful for our analysis.
Thanks.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.