Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Power Delivery possibilities

Hello,        I am creating a board using the STUSB4500QTR and I saw something on a video that confused me.  I want to use the IC to take in 100W (20V/5A) and output three different voltage rails: 3, 3.3 and 3.7.  Each will have a fairly large curren...

Resolved! Download STSW-WPSTUDIO

I bought the STEVAL-WLC99RX evaluation board for the STWLC99 Qi 1.3 compatible receiver and cannot find a location to download the GUI to program/monitor the receiver. The page that I am pointed to (https://www.st.com/en/embedded-software/stsw-wpstud...

sedmonds by Associate
  • 4358 Views
  • 7 replies
  • 1 kudos

SPV1040 IC Burns

@TDK , @Peter BENSCH  we are facing SPV1040 IC failure (burns) in the field, after around 3 months of installation, attached schematic and our solar Panel speciation Voc:4.55V, Vm:3.85V, ISC:1026mA, Im:950mA.Battery spec - 9000mAh, 4.2V Lithium ion.

Resolved! STWBC86 use for bi-directional communication

STWBC86 TX can be use for bi-directional communication, when rx send PP-packet as QI defined, STWBC86 update to 1251 version and use GUI to read i2c reg address 0x0100, and it can read RX PP-packet. https://github.com/STwirelesscharger/STSW-WPSTUDIO/...

willzhou_0-1708334043723.png
willzhou by ST Employee
  • 7147 Views
  • 8 replies
  • 7 kudos

MASTERGAN1TR failing and smoking at 100VDC

We are using 2 MASTERGAN1TR to drive current across an inductor.We are seeing damage on the body of the chip nearest the low side ground connection with a PWM Frequency of 250KHz and a 12% duty cycle.Before the chip fully fails the current decreases ...

bwefers by Associate II
  • 267 Views
  • 0 replies
  • 0 kudos

VNQ9080 to controll auxiliary lights of my motorcycle

Hi all. I've made a dedicated PCB that should control auxiliary lights of my motorcycle. I use CANBUS information by MCP2515 module and using Arduino Nano digital output pins to directly control input pins of VNQ9080. I assembled all elements on the ...

stojank by Associate
  • 518 Views
  • 1 replies
  • 0 kudos

powerStep01 Active Position Tracking

Is there a way to read the motor position while it's moving, such as with a command like "run," "goto," "move," or any other command from the Powerstep01? Does the motor need to be stopped for the motor position to be read correctly? Currently, when ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.