Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Mystery IC number ?

Hello allI don't know if this is the right sub-forum, I chose the one that seemed the closest.I've been spending a bunch of time trying to find the part number of a seemingly simple IC, but just hitting walls. I've Googled using the manufacturers nam...

20251007_132429.jpg
PLew by Associate II
  • 985 Views
  • 6 replies
  • 2 kudos

Precision voltage reference with low 1/f noise

Hi all, I am looking for two voltage references to produce two rails ( positive and negative) with low frequency noise.The voltage reference does not need to have a tight output voltage accuracy and long term precision. It needs to be stable over a 1...

Immagine 2025-02-05 123152.jpg
Tommino by Senior
  • 5701 Views
  • 7 replies
  • 0 kudos

Resolved! LM317 adjustable voltage setting question

I'm reviewing the datasheet for the LM317 linear regulator, and it lists the equation for calculating voltage as:VO = VREF (1 + R2/R1) + IADJ R2If I plug in the numbers from my circuit (and neglect the error calculation), I get:1.25 * (1+(1400/400)) ...

gdecker1 by Associate II
  • 534 Views
  • 1 replies
  • 0 kudos

L6566bh Flyback Startup failure

I have followed the design attached in PDF. It is from ST designsuit.I have used MYRRA 75032 flyback transformer. (Datasheet Attached)Optocoupler 140105146000 with CTRmin - 50%, CTRmax - 150%.So now problem is I am not able to get continuous Vout fro...

Rajesh_J_4-1759908394615.jpeg Rajesh_J_5-1759908530633.jpeg Rajesh_J_0-1759908046874.jpeg Rajesh_J_6-1759909916995.jpeg
Rajesh_J by Associate
  • 410 Views
  • 0 replies
  • 0 kudos

Resolved! Demo Code of AEK POW BMSLV

Hi, I wanted to ask the group if the demo code "SPC58EC - AEK_POW_BMSLV application for discovery" already includes automatic cell balancing, or if it doesn't, or if it needs to be enabled somehow. I was also interested in knowing if there was a GUI ...

antonio0101_0-1759412267073.png

Resolved! STSW-WBC2STUDIO

   Hello STMicroelectronics Support Team, I would like to make a custom wireless power transfer based project. I was trying to download the GUI (STSW-WBC2STUDIO). I am planning to use STEVAL-WLC38RX and the STEVAL-WBC2TX50. Please send me the softwar...

G1 by Associate
  • 2434 Views
  • 1 replies
  • 0 kudos

Resolved! powerSTEP01 motor current unstable in one direction

I have a powerSTEP01 driving a stepper motor with the coil current set to 2A. However, the current flowing in the coils is unstable when it is flowing in one direction:Sorry about the image quality - I have an old 'scope, so had to use a photo ;)The ...

IMG_2335.jpeg
CTapp.1 by Senior III
  • 740 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.