Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

EVM Board(steval-isa109v2, STBB2JAD)

I have checked input-current on the EVM Board(steval-isa109v2, STBB2JAD) with output-current is no load. Please refer below.​​- EVM Board Spec. Input voltage: from 2.3 V to 5.5 V Output voltage: 3.3 V Output current: 800 mA Operating frequency: 3 MHz...

BBQ by Associate II
  • 586 Views
  • 0 replies
  • 0 kudos

Resolved! Getting Started with STEVAL - SPIN3202.

Hello, I got board STEVAL - SPIN3202 and i want to use it with BLDC motor. how i will get getting started with it? i even not found any example. can anyone direct me to that? Thanks.

TPate.2 by Associate
  • 2694 Views
  • 7 replies
  • 0 kudos

STEVAL-ISC004V1 why add D0? Can work at 48V?

HelloWe have buy a STEVAL-ISC004V1 the doc do not say the maximum voltage but by analizing the shematic i watch only the ST1S14PHR receive Vin then i think he can accepte 48VBut i have connect it to a 45V and i see D0 burn But no D0 on your shematic...

SFour.1 by Associate
  • 851 Views
  • 0 replies
  • 0 kudos

How to calculate Schottky rectifier diode Power? (STP2L40U)

Hi I use STPS2L40U in the buck-boost circuit. ​I read STP2L40U datasheet. It shows Schottky rectifier diode P=0.22xIF(AV)+ 0.06xIF(RMS) 2.I have three question.What are 0.22 and 0.06 meaning? Does IF(RMS) mean LX path current or others? P means power...

0693W00000FAb6kQAD.png 0693W00000FAb6aQAD.png 0693W00000FAei0QAD.png 0693W00000FAepnQAD.png
TSU.11 by Associate II
  • 932 Views
  • 0 replies
  • 0 kudos

Top Side Marking for STN3NF06L

Please advise if there's a PCN related to the top side marking for the part number STN3NF06L?Also please confirm if both top side marking is valid. Attached photo for reference. Thanks

igamoso by Associate III
  • 870 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.