2021-09-25 1:47 AM
Hello
The STC3100 IC clock setting. Is it possible to trim Rosc from the recommended value of 200K and to set the internal oscillator from 32KHz to a higher rate of ~64KHz which is under max of 70KHz?.
The request is to increase sampling rate of T and V from 2.0 seconds down to1.0 second. If possible, double the I current sampling rate timing too.
If possible, trimming the Rosc and not to use external clock input.
Thank you for your cooperative response
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.