2021-09-01 6:38 AM
Hello, I got board STEVAL - SPIN3202 and i want to use it with BLDC motor. how i will get getting started with it? i even not found any example. can anyone direct me to that? Thanks.
Solved! Go to Solution.
2021-09-01 8:03 AM
Hello @TPate.2 ,
You can start by downloading the X-CUBE-MCSDK, then select launch application under MC_SDK_5.4.7\Utilities\PC_Software\STMCWB\STMCWB.exe, then click on new project Application if any, NewProject->SelectBoards = Inverter then Control = STEVAL-SPIN3202.
After this Generation, will generate some code for you with the desired IDE.
If you want more details about program and tool, you can find some documentation under MC_SDK_5.4.7\Documentation, especially UM2374.
BR,
Bruno
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2021-09-01 8:03 AM
Hello @TPate.2 ,
You can start by downloading the X-CUBE-MCSDK, then select launch application under MC_SDK_5.4.7\Utilities\PC_Software\STMCWB\STMCWB.exe, then click on new project Application if any, NewProject->SelectBoards = Inverter then Control = STEVAL-SPIN3202.
After this Generation, will generate some code for you with the desired IDE.
If you want more details about program and tool, you can find some documentation under MC_SDK_5.4.7\Documentation, especially UM2374.
BR,
Bruno
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2021-09-01 10:17 PM
i followed steps of STMCWB. but when i am going to connect serial port in Motor Monitor 3.6 in UM2374. it shows "Connection failed! No response. Check communication cable, the power on the board or the baudrate." also i saw code while(1) in main() is empty. was i made any mistake or i need to write code there?
2021-09-02 12:13 AM
Hi @TPate.2 ,
for more details on STEVAL-SPIN3202 board configuration you can refer to the "Documentation Tab" in the product page:
Let me know if these info help you.
2021-09-02 12:52 AM
@TPate.2 please make sure you select appropriate port and baud rate to 9600 baud
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2021-09-02 12:53 AM
Yes, main code is empty, UART and MC tasks executed under systick()
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2021-09-22 5:56 AM
Hi @TPate.2
Did you check the baud rate setting?
Were you able to play with the STEVAL-SPIN3202?
If so, remember to "Select as Best" label in the proper reply to your original question.
2021-09-28 10:57 PM
hi,
make sure to connect the power supply too, beside the usb cable
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.