Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STC3115 RemTime stays -1

Hello Everyone,I am using an STC3115 for managing the NCR18650B battery in my application. (In this setup the temperature measurement is not used because the battery doesn't have a THM pin. That's why the temperature value is 180.)My problem is the ...

0693W00000FDVkpQAH.png
AVajd by Associate II
  • 679 Views
  • 0 replies
  • 0 kudos

Resolved! STSPIN840 PWM and PH signal management

For PH 0 & PWM 1, is the current OUT1 -> OUT2 correct?I think the picture below is an act for the above case. If my guess is wrong, how do I rotate the motor in the reverse direction?

0693W000005AjXFQA0.png 0693W000005AjXeQAK.png

STPM34 primary voltage/current reading issue.

Hi,So I got myself an EVALSTPM34 and decided to test it out with the evaluation software given by ST.According to the STPM34 datasheet/user manual to read the primary channel current and voltage I have to read the 48th register which contains the dat...

0693W00000FDL4lQAH.jpg 0693W00000FDLArQAP.jpg 0693W00000FDLAhQAP.jpg
PMaha.3 by Associate
  • 1083 Views
  • 0 replies
  • 0 kudos

Resolved! How can we increase soft start time for VIPER319XDTR?

Dear sir, We have followed STEVAL-VP319X1B development board schematic for converting 110V/230V AC to 5V DC. In one of board we found that inrush current limiting resistor is burn out. We have followed same part number for resistor which is in develo...

Kshah.21 by Associate II
  • 11026 Views
  • 14 replies
  • 0 kudos

4 arms half-bridge symmetrical converter design

We want to control a 4 phase variable reluctance machine. For this we need to make (or buy) 4 arms half-bridge symmetrical converter with the following characteristics:Max current of the DC bus: 62 AMax DC bus voltage: 25.2 VMax PWM frequency: 30 kHz...

YSAAD.1 by Associate
  • 1045 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.