Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! I can't find a special component to repair a device. Can anyone help me. See details and photos below. Thanks in advance.

Here are pictures of the component I'm looking for.This comes from a control board for a rear light (Led) from an Aston Martin DB9 - 2005.There are 4 on the board and one of them is burnt.I can not find this component in the trade and impossible to f...

0693W00000FDtV0QAL.jpg 0693W00000FDtUbQAL.jpg 0693W00000FDtU7QAL.jpg 0693W00000FDtTdQAL.jpg
DBENS.1 by Associate II
  • 1548 Views
  • 5 replies
  • 0 kudos

LED1642GW LED's flicker during brightness changes.

Testing the LED1642GW using the X-NUCLEO-LED16A1 expansion board. I appear to have the communication working using the digital keys for LE on a GPIO output and a SPI interface. I can read and write the configuration register and write brightness valu...

DKeny.1 by Associate
  • 1093 Views
  • 2 replies
  • 0 kudos

Resolved! EVALSTRDRIVE101 firmware example is missing.

Since I do not want to use MCSDK but embedd the motor control in my own firmware I would like to have a firmware example for EVALSTRDRIVE101. Unfortunately the firmware example from ST does not seem to be available at this link https://www.st.com/en/...

meltabo by Associate II
  • 1986 Views
  • 3 replies
  • 0 kudos

Hello, We are using similar design of STEVAL-ISA203V1 with different transformer: CoilCraft POE600F-12LD. We see that there is very high current on the shunt resistors.

The peak on the resistors is about 2V, and we are using 3 parallel 0.1ohm resistors -> causing the device not working and infinity retries.We made a lot of experiments but for now, without any success.Any suggestions?I didn't find the datasheet of Co...

EOvad.2 by Associate
  • 706 Views
  • 1 replies
  • 0 kudos

We have a requirement of power line communication temperature data measurement by 7580 IC Nucleo board. Initially we found this is very supportive, but the same time we found the ST board programming is bit difficult. Hence, now we are using Arduino board

We have a requirement of power line communication temperature data measurement by 7580 IC Nucleo board. Initially we found this is very supportive, but the same time we found the ST board programming is bit difficult. Hence, now we are using Arduino ...

SE.1 by Associate
  • 728 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.