2021-10-27 11:35 PM
Since I do not want to use MCSDK but embedd the motor control in my own firmware I would like to have a firmware example for EVALSTRDRIVE101. Unfortunately the firmware example from ST does not seem to be available at this link https://www.st.com/en/embedded-software/stsw-drive101.html
Do you have any idea where I can find a firmware example for this Board?
Thanks for your support!
Solved! Go to Solution.
2021-10-28 12:45 AM
Welcome, @meltabo, to the community!
Sorry for the inconvience - the software has been moved to the MCSDK, you can find it in X-CUBE-MCSDK-Y or newer, where you can use it to start a new project.
Good luck!
If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.
/Peter
2021-10-28 12:45 AM
Welcome, @meltabo, to the community!
Sorry for the inconvience - the software has been moved to the MCSDK, you can find it in X-CUBE-MCSDK-Y or newer, where you can use it to start a new project.
Good luck!
If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.
/Peter
2021-10-28 1:06 AM
One more question. Since I'm not allowed to work with Motor control library, I need to generate the output signals for EVALSTDRIVE101 on my own. Apparently it does not work when I put PWM signals on INx and 3.3V on ENx. (Of course I selected mode INx/ENx). From what I read in the datasheet, this should be exactly what I need to do, enable all the half bridges ENx by putting 3.3V and then feeding the PWM signals on IN_U, IN_V and IN_W, which correspond to the voltages for each phase. Subsequently STDRIVE101 is generating the signals GLSx and GHSx in the correct way.
What am I missing?
In MCSDK I can only find examples where INxH/INxL is enabled. I try to do pattern matching, but there is no examble for ENx/INx mode of the STDRIVE101.
2021-10-28 1:12 AM
The original question has been answered, so please open a new thread for further questions.
Thank you very much!
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.