Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to configure POWERSTEP01 ocd_th in current mode?

Hi,Using IHM03A1, I try to drive a 48V-9A motor. I've set up the POWERSTEP01 driver in current mode, with default registers values, which works nicely but with low torque. Now I want to increase current up to 9A. I've changed IHM03A1 R1 and R2 resist...

BL1 by Associate II
  • 1924 Views
  • 3 replies
  • 0 kudos

Linux kernel driver for the L9823 ST chipset (digital output)

Hi Team,   We are using the L9823 chipset and it is interfaced with imx9qm SOC over spi.   Now, I gone through the code of linux kernel but I cann't see any linux kernel driver for L9823 ST chipset.   can you please help us to get the linux kernel dr...

DS.6 by Associate
  • 1035 Views
  • 1 replies
  • 0 kudos

ESC Commutation, Noise and Max. Speed Problem

Hello Sir or Madam,We have designed an ESC according to STEVAL-ESC002V1 and used ST's 6Step_Library. In our application, There are commutation, noise and maximum speed problem. MCU and gate driver is STSPIN32F0AMOSFET is STL220N6F7Switching frequenc...

Why 400V 800W PFC with L4984D function ok when the load is resistive but not when the load is a switching with a transformer?

Hello, I designed and manufactured a PFC circuit with a L4984D for 400V 800W output. I tested it until 860W with a resistive load and function ok. I need to power with it a 600W, 400V to 24V DCDC. This second step consist of a full bridge with a tran...

EBaye.1 by Associate
  • 966 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.