Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
Hey guys,I would appreciate your thoughts on this. I have presently implemented 6 PWM schemes to modulate the 2-level 3 phase inverter I am using to control my BLDC motor in a simulation. Those PWM schemes are shown in the figure below I observed tha...
We had the following queries:1.Pins LIN is mentioned as active low.Will the low side PWM output from driver be high when input to LIN pin is low?2.VCC is mentioned to be between 10-20V.But all input pins(SD,HIN,LIN) are operating at 5V level.Is there...
I have a question, I am presently working with a bldc motor. And I also did a simulation on matlab.So I observed this:1. when I applied a certain load torque (let’s say 0.4Nm), then I give my controller a set point speed (400RPM) the controller is no...
Using SPINFamily Evaluation Tool 3.2, STnucleo-f401re and IHM03A1, I try to drive a 48V-9A motor. In SPINFamily interface, I choosed current mode and tried to set run current to 9A. But an error show up in the interface: "Power dissipation on sense r...
Hello.1- We want to add USB Power Delivery to an existing converter which can deliver 2x 5.1 V/3A from an unique power stage (isolated converter with one transformer, one regulator IC, etc.).The PD-controller has to meet the following requirements:-N...
I have an EV that was converted from internal combustion engine to electric using lead/acid batteries. It's been upgraded to LiOn cells but needs a battery management system to be safe and usable. I know several others with the same need. The L996...
Back emf from the motor is entering into other digital causing some issues. How can i avoid/isolate this back emf on STEVAL-spin3201
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.