2021-11-20 1:17 AM
Hi
I'm running a SMPM motor and i have resonace problem in mechanical system resonance frequencies: 1.2Hz 2.4HZ 4.8HZ and in other frequencies everything is ok. The resonance is low it noload but worse in full load.
I ckecked current controller,angle,speed controller is ok and it's not depended to switching frequency.
I can't see vibration in speed feedback(that has 0.01hz resolution) and everything is smooth.
Do you have any idea about this problem?
2021-11-30 7:11 AM
Hello @mhass.1 and welcome to the ST Community.
For better understand what happens, could you share more details?
> I can't see vibration in speed feedback(that has 0.01hz resolution) and everything is smooth.
How did you measure the motor resonance?
What kind of mechanical load are you using?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.