2021-12-02 9:23 PM
We had the following queries:
1.Pins LIN is mentioned as active low.Will the low side PWM output from driver be high when input to LIN pin is low?
2.VCC is mentioned to be between 10-20V.But all input pins(SD,HIN,LIN) are operating at 5V level.Is there any internal generation of 5V?.
Also should the SD pin be pulled up to an external 5V ?
3.Please share the unused pin recommendation for CP+ and CP- pins.
4.Can the deadtime be controlled by varying RDT?
5.Kindly share the layout guidelines for the ic as well.
Solved! Go to Solution.
2021-12-03 4:11 AM
Welcome, @HV Ku.1, to the community!
Regards
/Peter
2021-12-03 4:11 AM
Welcome, @HV Ku.1, to the community!
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.