Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! EVAL6498L Bootstrap diode internal to the chip?

Hi there, regarding EVAL6498L, is it necessary to mount the diode D1 (represented as not mounted in the schematic diagram)? or is D1 not necessary because the bootstrap supply diode is already included inside the 6498 integrated circuit?Thank you

Lello by Associate II
  • 2231 Views
  • 4 replies
  • 0 kudos

Resolved! Measured output current lower than asked value

Hi, Using SPINFamily Evaluation Tool 3.2, STnucleo-f401re and IHM03A1, I'm trying to drive a 48V-9A motor.On IHM03A1, I add 15mOhm/3W resistances in parallel of R1 and R2, so R1 and R2 value is now 13mOhm. According to @Cristiana SCARAMEL​ recommanda...

BL1 by Associate II
  • 2142 Views
  • 6 replies
  • 0 kudos

Resolved! Is there any off the shelf software available that will perform sensorless velocity measurement using back emf of a brushed DC motor?

I would like to investigate velocity control of a brushed DC motor using the STSPIN240/250 devices. The motor velocity can be measured using the back emf from the motor. Does anyone know if there is any off the shelf software for this?I notice the X-...

SCrum.1 by Associate III
  • 2285 Views
  • 4 replies
  • 1 kudos

Resolved! Temperature threshold raised

Hi, Using SPINFamily Evaluation Tool 3.2, STnucleo-f401re and IHM03A1, I try to drive a 48V-9A motor.On IHM03A1, I add 15mOhm/3W resistances in parallel of R1 and R2, so R1 and R2 value is now 13mOhm. In SPINFamily interface, I choosed current mode, ...

BL1 by Associate II
  • 2362 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.