Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
Compiler/IDE CCS STUDIOTarget TIVA4c129Any help or hind from any end is appreciable, We are informing our thanks in advance.SchematicsCode Snippet
I have a STEVAL - Spin3202 board. I want to use this board and ST motor control workbend to control my BLDC.I use ST motor control workbend to generate code ( for KeilC). When I try to load project to Spin3202 an error appears: "No target connected"W...
HiWe observe sudden changes and flickering especially at low level luminosity.attached oscilloscope capture_1 is taken at one of green LED channels. During the dimming cycle, the ghost pattern causes momentary flashes in LED brightness.again oscillos...
For the ULN2002, ULN2003, and ULN2004 the datasheet gives detailed information depending on the continuous collector current, but no such info is given for the ULN2001.
Hi All, I tested the motor driver STSPIN840. I'm able to limit the current through the motor. But i dont see the Fault Pin going down to zero if the driver limits the current. If i do a short circuit on the output the Fault Pin goes down to Zero. Wha...
I wasn't sure where to post this request for the STNRG digital control IC example files so Power Management is my guess.There is a link to download 5 sample files for the STLUX chip and 3 more for the STNRG digital controller eval boards. In the avai...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.