Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

L6599 or L6699 as Full Bridge controller?

Hi,I am already using the L6599 as a HB LLC controller and I am trying to achieve higher output powers, however my input supply voltage is only ~30V. Already primary side currents are high. In order to bring these to realistic levels I really should ...

Resolved! Output capacitor type for use with LD1117

Dear Forum members,Could you please confirm if the LD1117 is specified to work with ceramic output capacitors?Unfortunately the datasheet makes no mention of capacitor type or ESR requirements.Thank you

Bvan .11 by Associate II
  • 5606 Views
  • 7 replies
  • 0 kudos

Problem with pin status after power on

Hi, I am solving the backlight of the display, which is controlled by a pin, but the problem is the state between power on and initialization, when the display flashes before the pin is initialized. This happens with both positive and negative contro...

0693W00000NqoXVQAZ.png
Filipx.87 by Associate II
  • 1163 Views
  • 1 replies
  • 0 kudos

STSPIN32F0,Vreg12(Pin6) cannot output DC voltage stably.

Problem Description.After reflow soldering the circuit board, after visual inspection to exclude the problem of soldering quality, the power test on the tooling (DC 12V power supply, the output of the circuit board is not connected to the load). Outp...

0693W00000NpWjRQAV.jpg

SPV1050 SPICE model

Hi All, we need t simulate the SPV1050 on LTspice, but the provided model generates the "Too few nodes" error. Is there any specific version of LTspice required to run the model without errors? Is there another spice software recommended for the mod...

AAzai.1 by Associate
  • 2143 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.