2022-05-31 11:51 AM
Dear Forum members,
Could you please confirm if the LD1117 is specified to work with ceramic output capacitors?
Unfortunately the datasheet makes no mention of capacitor type or ESR requirements.
Thank you
Solved! Go to Solution.
2022-05-31 12:27 PM
Welcome, @Bvan .11, to the community!
The LD1117, which is quite 20 years old, is a low-dropout regulator that requires an output capacitor of at least 10µF and an ESR (equivalent series resistance) of at least 0.3 ohms. 20 years ago, they simply used an electrolytic capacitor whose ESR was large enough. In addition, the large capacitance values of ceramic capacitors were not yet available at that time, so they were not mentioned in the data sheet.
If a tantalum capacitor is out of the question (there is massive criticism of the circumstances of tantalum mining), you can also use a ceramic MLCC, but then you should connect a resistor of approx. 0.5-2 ohms in series as an artificial ESR.
Does it answer your question?
Regards
/Peter
2022-05-31 12:26 PM
https://community.st.com/s/question/0D53W00000Aaci7SAB/ld1117s50-output-capacitor
2022-05-31 12:27 PM
Welcome, @Bvan .11, to the community!
The LD1117, which is quite 20 years old, is a low-dropout regulator that requires an output capacitor of at least 10µF and an ESR (equivalent series resistance) of at least 0.3 ohms. 20 years ago, they simply used an electrolytic capacitor whose ESR was large enough. In addition, the large capacitance values of ceramic capacitors were not yet available at that time, so they were not mentioned in the data sheet.
If a tantalum capacitor is out of the question (there is massive criticism of the circumstances of tantalum mining), you can also use a ceramic MLCC, but then you should connect a resistor of approx. 0.5-2 ohms in series as an artificial ESR.
Does it answer your question?
Regards
/Peter
2022-05-31 12:30 PM
Thank you very much Tesla,
The link you provided to the other question/answer was very useful.
Regards
2022-05-31 1:16 PM
Hello Peter,
Thank you very much for your detailed response.
I suspected something like this.
Regards
Ben
2022-05-31 1:19 PM
Great!
If the problem is resolved, please mark this topic as answered by selecting Select as best under your preferred answer. This will help other users find that answer faster.
Good luck!
/Peter
2022-05-31 2:18 PM
Take a look on LDL1117 - it's a newer and better design. Much better specifications and the required capacitors and ESR are documented good enough.
If something goes wrong, tantalum capacitors tend to fail with a short circuit and explode. Generally try to stick with a ceramic and aluminium electrolytic (especially the polymer) capacitors.
2022-05-31 9:54 PM
Hello Piranha,
Thank you for the suggestion, Indeed it does looks like a better option.
Regards
Ben
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.