Resolved! diode identification
I would like to identify the following two diodes, please.
Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
I would like to identify the following two diodes, please.
Hello,I want to adapt the STGSH50M120D to the circuit I already have working, but I have a question about pins K1 and K2. Will there be any problem with the STGSH50M120D if I don't use K1 and K2, leaving them disconnected?
Hi,We are using STSPIN958 for BLDC control, and under 33V, 2A, when external force applies to servo, and the current goes up to about 2A, the chip burns before the thermal shut down kicks in.I would also like to know the value of "Tsd" delay timing p...
Dear ST Community and Experts, I am facing a persistent SPI error (SPIE bit set) issue with the VN9D5D20FN high-side driver and would appreciate your help in troubleshooting. 1. Problem Description: I am attempting to write to specific control regist...
HI! We have from time to time defect High Side Driver. Most of the defects occur after the first few power on cycles. The High Side Driver and the RGND Resistor (120Ohm) gets really hot. The resistance between GND and the Status Pin is then much l...
Hello! I am building a 50-600Vin flyback converter using the altair04-900 to power an LED as a student project. Due to the very light load I expect it to work in Burst mode. Currently I am looking for an adequate transformer. On this regards my quest...
This is to turn on MOSFETs that operate above 5.2V supply of the Boost regulator. I have followed a forward converter guidance roughly in one of the application notes, but I have not used a transformer but placed a high value resistor in the voltage...
Hello, We are looking to use the Wlc38 in Bi-directional mode alternating between RX and TX digital pings. We are wondering how much power consumption the digital ping takes and for what duration so we can calculate power consumption of pinging at va...
Hello everyone,I am finding to drive for 4 cabin lock. For this, VNxxx or VNQxxx series help me. I don't need high current. It is 1 amper per channel(per output. I'm looking for a chip that will not cause any supply problems and will be produced con...
HiIs it possible to bypass the boost by applying a 5V voltage directly to BSTOUT (VLXBST is left unconnected)?Thank in advance for your reply
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.