2025-11-04 6:36 AM
Hi
Is it possible to bypass the boost by applying a 5V voltage directly to BSTOUT (VLXBST is left unconnected)?
Thank in advance for your reply
Solved! Go to Solution.
2025-11-05 12:47 AM
Hello Spub,
The proposed idea does not work as expected. The boost bypass monitors the input voltage (Vin). If the input voltage (Vin) exceeds the boost output of 5.2V, the bypass activates when the input voltage (Vin) reaches the threshold of ~5.25V.
Regards,
Vincenzo
2025-11-05 12:47 AM
Hello Spub,
The proposed idea does not work as expected. The boost bypass monitors the input voltage (Vin). If the input voltage (Vin) exceeds the boost output of 5.2V, the bypass activates when the input voltage (Vin) reaches the threshold of ~5.25V.
Regards,
Vincenzo
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.