Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

PowerSTEP01 self-contradicting datasheet

The PowerSTEP01's datasheet says on page 34 that MIN_SPEED is 12 bits wide.On page 37, it is described as 13 bits wide.I suppose that 13 is correct, from code I've read online, but a confirmation (and fix) would be nice. I cannot see the low speed op...

Test result data for 5V output device LDK220U50R

Hello Team,We have selected part no: LDK220 and LDK320 with a SOT-89 footprint for one of our applications. We have referred to the complete datasheet, but we have not found the test results for 5V output category devices, like the voltage dropout of...

JYada.1 by Associate II
  • 475 Views
  • 3 replies
  • 0 kudos

STEVAL-ISD01KCB

I've been looking at the STEVAL-ISD01KCB, and I saw in an image that it has some capacitors between pins 8 (-DC) and 9 (+DC). What is the value of that capacitor? Is it necessary to include it? I ask because I've noticed that this capacitor slightly ...

Resolved! Viper318HD

 I have  design Buck  converter with Viper318HD ,With below specification:Vin:(85 to 265)VACVout=12VDCIout=500mAAnd i not follow recommended   Commponents   value  which  Are mentioned in Edesign tool,  i use  components which  are availble  with me....

Rahmaa_0-1762881720207.png
Rahmaa by Associate II
  • 1183 Views
  • 8 replies
  • 0 kudos

Is it possible to parallel multiple STEF01 e-fuses?

I have a design running on 24V SLA batteries using STEF01 fuses for protection of the lower powered rails and an LT4356 using external MOSFETs for a 25Amp rail. That 25A rail is giving me headaches. Staying within the SOA of the MOSFETs is not that e...

bart2 by Associate II
  • 323 Views
  • 0 replies
  • 0 kudos

power source

Hello, (L6562DTR)I have encountered some problems when using this chip and hope to get some suggestions from you;  ”The PF output voltage of 480V FC load is 0.7435“   The power input voltage is 250V-528VAC, with PFC+ flyback. The PFC BUS voltage is 7...

liwei11 by Associate
  • 414 Views
  • 0 replies
  • 0 kudos

Resolved! Change PDO3 to 15V, 1.5A don't work

Hello Everybody, I'm new in this place. I use an Evalboard ISC005V1 with STUSB4500 and an dedicate MCU to manage I²C port. I wanted to change the configuration of the PDO3 from 20V to 15V. I select PORT3 ( write 3 in 0x70 register ) I configure DPM_R...

LEGLAUDE by Associate
  • 488 Views
  • 1 replies
  • 0 kudos

EVALSTGAP2HDM

Hi, We have been testing our H-bridge on 2 EVALSTGAP2HDM with IPP026N10NF2S MOSFETs. The gate resistances are as per the EVAL board. We are seeing huge ringing on the gate signals for the low side FETs on both boards with no load connected. The high ...

arjunkc by Associate
  • 573 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.